Compatibility of Koolance Hard Drive Water Cooling Products
Koolance Hydra-Pak hard drive coolers are universally compatible with most 3.5" hard drives. They are mounted using the 4 screw holes on the bottom side of the drive. Bus interface (SATA, IDE, SCSI, SAS) is irrelevant for compatibility.
Coolers are available for single (HD-50-L06) or dual (HD-57, HD-60) hard drive cooling. The dual drive coolers can be sandwiched between dual hard drives, with one drive mounted upside-down.
Whether one, both, or neither liquid cooler can be used depends upon the computer chassis' method of mounting hard drives.
The first requirement is sufficient distance between installed hard drives. For the HD-50-L06 water block, there should be at least 3/8 inches (10mm) of clearance below a hard drive to liquid cool it. For the HD-57 water block, there should be at least 0.9 inches (23mm) for a single hard drive, or 0.7 inches (17mm) for cooling dual hard drives. And for the HD-60, there should be at least 5/16 inches (8.5mm) of clearance between hard drives.
If space is unavailable, consider spacing out hard drives to make room. A hard drive can also be mounted upside-down to allow for a liquid cooler to attach above it.
The second requirement is a compatible hard drive mounting method. In general, hard drives are mounted inside computer chassis with side screws, rails, or individual trays:
Screw-Mounted Hard Drives
Rail-Mounted Hard Drives
Tray-Mounted Hard Drives
Screw and rail-mounted drives are generally compatible with any Koolance hard drive liquid cooler (provided there is room). However, tray-mounted drives are not compatible with Koolance HD-57 or HD-60 coolers because the tray interferes with the dual "sandwich" mounting method. If room is available between drives, the single Koolance HD-50-L06 may work in this situation.
Depending on the nozzles chosen for it, the HD-57 and HD-60 water blocks may not work in all systems. If your chassis places the hard drive connections near a side panel (perpendicular to the front), make sure the selected cooling block nozzles will fit. Each nozzle page has a "diagrams" button with dimensions.
Whichever Koolance product is used, water blocks are not mounted directly to the drive bay. They attach to the drive, which is then secured to the chassis by traditional means.
For example, when using the Koolance HD-57, only one of two hard drives is mounted to the chassis; the other rests above or hangs below the liquid cooler.
Drive Trays with Koolance HD-50-L06 Blocks
Drive Rails with Koolance HD-55-L06 Block
Drive Rails with Koolance HD-57 Block
Drive Rails with Koolance HD-60 Block







GPU Hole Spacing
Quick Disconnect Help
VGA Card Photos