Compatibility of Koolance RAM Water Cooling Products
NOTE: To install Koolance RAM cooling products, the memory's original heat spreaders or heat sinks (if any) should be removed in order to fit. This is also to prevent damage to the Hydra-Pak during installation, and to provide superior cooling by getting water flow as close to the memory as possible. If your memory sticks have heat spreaders, please verify these can be physically removed before purchasing a Koolance memory cooler.
Koolance RAM-35
The RAM-35 is unique in that there is no particular limit to the number of consecutive DIMM slots which can be cooled. Using one RAM-35 cooler per memory slot, directly adjacent banks are linked with Koolance RAM-35 connection nozzles (described in greater detail in the user manual).
Due to the special and technical nature of the
RAM-35, it is
Koolance RAM-33
Like the RAM-35, the RAM-33 has no particular limit to the number of consecutive DIMM slots which can be cooled. The RAM-33 has regular perpendicular nozzle sockets, so practically any type of connection can be made using traditional tubing methods. A specific sliding connection nozzle can be used to easily connect blocks.







GPU Hole Spacing
Quick Disconnect Help
VGA Card Photos