|
| |
|
Sept. 22, 2003 |
P-4 Northbridge Spring Clip
The thin retention spring included with CHC-A05 and CHC-A01
Chipset Coolers is for mounting the chipset to Pentium 4 Northbridge
motherboard chipsets. It is not required to mount the cooler on any
other type of chip. |
|
|
Sept. 8, 2003 |
Upcoming GeForce FX 5900 / Radeon 9800 Pro Support
The current CHC-A05 gold chipset will operate with ATI Radeon
9800 Pro cards, but not the nVidia GeForce FX.
Koolance will release a high-performance video chipset cooler in
October which is expected to provide a significant increase in
efficiency for these high-level cards.
Please continue to check the homepage for product announcements. |
|
|
May. 12, 2003 |
Xeon Adapter Incompatibility with some Tyan Motherboards
Some Tyan dual Xeon 603/604 motherboards have begun including a new
plastic mounting clip style which will not fit the Koolance Xeon
adapter.
Since the new clip does not appear to be model-dependent at this
time, we are not yet able to list incompatible boards.
Tyan's website includes user manuals which still feature the
earlier (compatible) style of Xeon plastic bracket. |
|
|
Apr. 29, 2003 |
New User Manual
Now available is a completely rewritten User Manual for Koolance
products (in color). This new format may not be included with
Koolance systems for at least 4-6 weeks, but you can download it now
from the manual
page.
The new style should provide even easier instructions on the setup,
installation, and maintenance of Koolance systems and liquid
coolers.
NOTE: The "Universal User Manual" includes all current Koolance
products, including: PC2-601, PC2-901, Exos, RM1-4U, and all
Coolers. You will not need to download the cooler installation
guides separately. |
|
|
Feb. 4, 2003 |
Using Alternative Components in a Koolance System will Void the
Warranty
As mentioned in the User Manual's
warranty, using
alternative manufacturers' parts in a Koolance system will void the
system warranty. This includes everything from coolers to pumps.
Our systems are designed to operate with pre-specified components.
Pumps which are too fast or too slow may result in an inefficient
flow rate through the heat exchanger and potential system damage.
CPU or chipset coolers which use an incompatible metal type or alloy
may result in a corrosive chemical reaction. Fans which do not
provide sufficient airflow to the heat exchanger over the voltage
range given by our control board may result in potential system
damage.
Koolance does not offer technical support for warranty-voiding
procedures or modifications. Please see the
FAQ for more
information. |
|
|
July 10, 2002 |
Applying Hard Drive
Thermal Material to the Spindle Motor
The User Manual specifies applying thermal encapsulate to the
primary semiconductors and spindle motor of the hard drive. The
encapsulate material should not be applied to the motor if
there is an opening in the center (See
Example). The thermal material can cause additional noise, and
may interfere with the drive's operation. In situations where the
material has already been applied, we recommend cutting a hole in
the encapsulate to free this area. |
|
|
June 21, 2002 |
New PC User Manual
Version 1.07 includes more details on installation of the CPU-200
cooler, and includes the new hard drive revision (which lacks a need
for the steel containment plate). If you have received a manual
prior to 1.07 with your Koolance case, please see the
downloads
page for updated installation instructions. |
|
|
June 3, 2002 |
Hard Drive Cooler Revision
The Hard Drive Cooling Plate has been altered so that it no longer
requires the steel "containment plate". One side of the cooler is
completely flush, so the thin plate is not needed to hold thermal
encapsulate against the drive. (It is still included with the
second hard drive kit.) |
|
|
May 14, 2002 |
Motherboard cooler compatibility
Although most boards will accommodate our liquid coolers, certain
combinations on specific motherboards may simply not fit. Some Epox
models (such as the
EP-8K3A and EP-8K3A+) for example, have a very short distance
between the northbridge chipset mounting holes and the CPU socket,
so that the mounting bracket of our chipset liquid cooler on the
motherboard may interfere with the CPU-200 cooler. In this case, we
recommend to use the CPU-100, or not to use a chipset cooler on the
northbridge. |
|
|
Apr 3, 2002 |
CPU-200 Cooler Installation
Sheet |
|
|
If you do not receive a small
installation sheet with your CPU-200 cooler, it can also be
downloaded from the support page. The instructions include important
information regarding thermal probe placement & bracket alignment,
which differ slightly from the installation of a regular CPU-100
cooler. |
|
|
Dec 5, 2001 |
Mounting Coolers onto the ATI
Radeon 8500 |
|
|
The ATI Radeon 8500 lacks heat
sink mounting holes found on the majority of video cards. Instead of
using the Koolance bracket, thermal adhesive or tape should be used
(such as
Arctic Silver Thermal Adhesive). |
|
|
Nov 27, 2001 |
Manual v1.05 Online |
|
|
While the latest User Manual is
being printed, those who have received the "1.05 Addendum" insert
can also download a full version from our support page. Changes
apply mainly to the liquid installation, providing more detail
through the process. There are other minor clarifications,
particularly in the Hard Drive & Configuration sections. |
|
|
Nov 19, 2001 |
USB Ports with Deep Front Bezel |
|
|
The original USB/Audio front
ports from the PC2-C do not fit correctly in the Deep Bezel.
Unfortunately, the chassis manufacturer does not make a shorter USB
bracket to fit the bezel design. The USB ports can still be utilized
after removing the rotating "door panel", but the audio ports are
unusable. We do not recommend purchasing the front USB ports with a
deep bezel. |
|
|
Oct 8, 2001 |
Use of CPU Shims |
|
|
Utilizing CPU Shims with
Koolance cases are unnecessary, and will void the system warranty.
Our patent-pending CPU bracket is extremely safe, placing even
pressure across the center of the processor as it's tightened. This
is unlike regular heatsinks, relying on asymmetrical pressure in
"leveraging-over" the mounting mechanism, which can damage a fragile
core. Using shims with our systems prevents the cooler from making
adequate contact with the processor, and may result in hardware
damage. |
|
|
Oct 1, 2001 |
Use of Alternative Liquids |
|
|
As the User Manual states,
adding alternative liquids to a Koolance system will void the
manufacturer warranty, and may result in serious damage to the
computer and hardware therein. This includes dyes, water (other than
what is provided in the included refill bottle), "Redline Water
Wetter", or similar products. We would strongly urge customers to
keep and to utilize the original liquid solution, as it has already
successfully undergone numerous efficiency and longetivity tests. |
|
|
Sept 20, 2001 |
Optional CPU Brackets |
|
|
Because of the many varieties
of upcoming socket designs, the standard K7/PIII bracket will be
included with each Koolance case (& individual CPU kit purchases),
and we will offer alternative CPU brackets as optional items. This
is not foreseen to be an enormous issue, since a typical CPU bracket
will probably cost around $3.00 (MSRP).
We are also working on a new P-4 bracket to fit Intel's new socket
478 "Northwood" processor, because the P-4 "Willamette" socket 423
bracket will not fit. The new bracket should be available soon. |
|
|
Aug 28, 2001 |
New PC Manual Posted |
|
For those who may want to
browse the new PC manual while waiting for more technical
information, it is now available for download. It also describes the
installation process, as it varies from our previous unit. |
|